i.MX6ULL board stuck at Starting kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL board stuck at Starting kernel

1,315 Views
michiel_tjampen
Contributor III

So i bought a Seeed I.MX6ULL board to gain experience with I.MX processors but the official image causes the board to go crash on starting the kernel. Then i managed to install an EVK image using uuu and that boots to log in (on console only) so i tried making my own image based on these (using 5.7 kernel) steps and after a lot cursing and learning new things i managed to get to a point where the board gets to 'Starting kernel' but then nothing happens.

U-Boot 2019.04-00676-gd447c486 (May 27 2020 - 05:26:26 +0000)

CPU: Freescale i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 49C
Reset cause: POR
Model: Freescale i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:
Error: ethernet@020b4000 address not set.

Error: ethernet@020b4000 address not set.

Error: ethernet@02188000 address not set.
eth-1: ethernet@020b4000
Error: ethernet@02188000 address not set.
, eth-1: ethernet@02188000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
Checking for: /uEnv.txt ...
Checking for: /boot.scr ...
Checking for: /boot/boot.scr ...
Checking for: /boot/uEnv.txt ...
Card did not respond to voltage select!
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
switch to partitions #0, OK
mmc1(part 0) is current device
Checking for: /uEnv.txt ...
Checking for: /boot.scr ...
Checking for: /boot/boot.scr ...
Checking for: /boot/uEnv.txt ...
1587 bytes read in 9 ms (171.9 KiB/s)
Loaded environment from /boot/uEnv.txt
debug: [dtb=imx6ull-seeed-npi.dtb] ...
Using: dtb=imx6ull-seeed-npi.dtb ...
Checking if uname_r is set in /boot/uEnv.txt...
Running uname_boot ...
loading /boot/vmlinuz-5.7.0-rc6-armv7-x5 ...
10250152 bytes read in 456 ms (21.4 MiB/s)
debug: [enable_uboot_overlays=1] ...
debug: [uboot_base_dtb=] ...
loading /boot/dtbs/5.7.0-rc6-armv7-x5/imx6ull-seeed-npi.dtb ...
38661 bytes read in 14 ms (2.6 MiB/s)
uboot_overlays: [fdt_buffer=0x60000] ...
debug: [console=ttymxc0,115200n8 root=/dev/mmcblk1p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 vt.global_cursor_default=0 quiet] ...
debug: [bootz 0x80800000 - 0x83000000] ...
Kernel image @ 0x80800000 [ 0x000000 - 0x9c67a8 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300c704
Modify /soc/aips-bus@2200000/epdc@228c000:status disabled
ft_system_setup for mx6

Starting kernel ...

Any tips on where to start looking? I found a page that said that it might actually keep going but just the console port being wrong. But it's the same as for the EVK image and that works fine...

I tried rebuilding the kernel to output more info but if it's not starting...

Or point me towards a different howto?

Labels (2)
0 Kudos
2 Replies

1,220 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Michiel,

We have not tested the 5.7 kernel image but you should try the 5.4 kernel BSP that is officially form NXP and is fully workable:

i.MX Software and Development Tools | NXP 

Regards

0 Kudos

1,220 Views
michiel_tjampen
Contributor III

Well I started from that but couldn't figure out how to alter it to different hardware, i'm not using an evaluation kit (and maybe related the usb gadget didn't start). But i'll give it a go again, noticed that i managed to overlook the separate docs package...

0 Kudos