AnsweredAssumed Answered

read cpu teperature at usespace in Windows 10 IOT Core on IMX8mq evk

Question asked by shen tom on May 28, 2020
Latest reply on Jun 4, 2020 by jimmychan

Hello Experts,

    

    I want to read cpu teperature at usespace in Windows 10 IOT Core on IMX8mq evk. For example, in Windows 10 IOT Core on IMX8mq evk I can type readcputemp in coammnd line to get to CPU temperature. I known how to get CPU temperature at kernel space. A simple sample like below:

+#define TMU_BASE    0x30260000

+    vaddr_t tmu_base = core_mmu_get_va(TMU_BASE, MEM_AREA_IO_SEC);
+
+    DMSG("======== is valid: 0x%08x, cpu temperatue: %d =====", read32(tmu_base + 0x100),  read32(tmu_base + 0x100) & 0xff );

 

But I hope can use  command line of windows IoT core in userspace to get this CPU temperature in kernel space.

 

Have any simplest example that I can do that

Outcomes