Hi,
I am getting the below error for the Phy IC DP83848 in RMII Mode in IMX8MMini
Error: ethernet@30be0000 address not set.
Below is the uboot log
-------------------------------------------------------------------------------------------
switch to partitions #0, OK
mmc1(part 0) is current device
flash target is MMC:1
Net:
Error: ethernet@30be0000 address not set.
No ethernet found.
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 2 1 0
switch to partitions #0, OK
mmc1(part 0) is current device
** Unable to read file boot.scr **
22999552 bytes read in 281 ms (78.1 MiB/s)
Booting from mmc ...
42981 bytes read in 9 ms (4.6 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300d7e4
--------------------------------------------------------------------------------------------------------------
How can we resolve it
Regards
Santhosh
Solved! Go to Solution.
This issue was solved by adding the MAC address,
setenv ipaddr 192.168.36.126
setenv serverip 192.168.36.10
setenv netmask 255.255.255.0
setenv ethaddr 00:a8:44:1f:1f:10
saveenv
Regards
Santhosh
This issue was solved by adding the MAC address,
setenv ipaddr 192.168.36.126
setenv serverip 192.168.36.10
setenv netmask 255.255.255.0
setenv ethaddr 00:a8:44:1f:1f:10
saveenv
Regards
Santhosh