Now,our customer is use i.MX8QXP L4.14.98 +SerDes MAX9286+MAX96705+Sensor AR1043 as Sourding 360 solution.
MAX9286 and MAX96705 should be found and initial is ok.But:
Error:write reg error:reg=0x3024,val=0x1.
mxc_isi_souce_fmt_init,set remote fmt fail!
Error: V4l2src0:Failed to allocate require memey.
So any advise for the problem?
TKs!
Hello,
You use AR1043 sensor,but your driver seems OV10635 sensor,so your remote device camera init failed.
Maybe you should config the driver for AR1043.
Thanks
Hi George
one can try to allocate more memory in dts file with "reserved-memory":
imx8x-mek.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------