Hi,
I had created project which was working fine. Now I have check-ed in project in wincvs(version management tool). But now when I check-out the project, and try to open ".mcp" file, its not getting loaded saying "resource file error 207012". I dont know what is resource file. Have anybody faced this problem before. Is there any solution since I have to use wincvs for version management.
Similar probelm is mentioned in
http://forum.soft32.com/mac/Resource-File-Error-207012-ftopict42034.html
Hello
Only thing I can think about is that wincvs did change something in the .mcp file (Which is a binary file) and CodeWarrior cannot open it any more.
When you are checking CodeWarrior projects in VCS software, my recommendation is to export the .mcp file to a .xml file (use entry File -> Export for that).
Then after you check out the .xml file import it into CodeWarrior to create the .mcp again.
CrasyCat