500瓦电源方案问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

500瓦电源方案问题

16,598 Views
bkl
Contributor I

你好!

目前我们公司使用TEA19161和TEA19162设计了一款500W电源。现状是输出为稳定电压,但电压值比设计值要高。通过看波形发现TL431的ref脚并非2.5V,而是一直处于震荡状态,且震荡中心值(波形中的直线)不足2.5V。请问可能的原因有哪些?

0 Kudos
16 Replies

16,446 Views
bkl
Contributor I

guoweisun

你好!

附件是电路图,请确认。

谢谢!

0 Kudos

16,446 Views
guoweisun
NXP TechSupport
NXP TechSupport

您的这个反馈回路再重新设计一下 431的静态工作电流计算下,参考UM10972 page27.

0 Kudos

16,446 Views
bkl
Contributor I

你好!

我根据240W的电路,修改电阻,使得输出57V时431的REF向外输出5uA电流,测试没有效果。后将TL431的KA电流增大到4mA以上,也没有改善。请问正常情况下ref是吸收电流还是提供电流?

0 Kudos

16,446 Views
guoweisun
NXP TechSupport
NXP TechSupport

如果是输出57V,反馈回路上必须得串联一个稳压管因为431的最大耐压36V左右,例如24V的稳压管,然后再去计算限流电阻静态工作点,静态工作点可以试着选择在2mA这样。

0 Kudos

16,446 Views
guoweisun
NXP TechSupport
NXP TechSupport

ref这个pin其实就是高阻抗的脚位,就是运放的输入端

0 Kudos

16,446 Views
bkl
Contributor I

你好!

我串联了一个36V稳压管,然后测得空载时,与光耦LED支路并联的电阻的电流为1864uA;光耦LED支路上加入一个限流电阻,该支路空载时电流为287uA,这样两个加起来2mA多点,即431的KA电流。此时KA电压为1.96V,是否也应为2.5V才正确?测得Vref为2.5V。空载时各点电压为直流,有稀疏可忽略的毛刺。加40W负载后,Vref,Vka等相关电压均为振动状态,形状和之前发的振荡波形类似,同时输出电压下降0.7V。增大功率后会继续下降。请问是否静态工作点还是不对?另外UM10972第26页,光耦LED并联了一个D302(BAS316),这个是否必须?作用是什么?

0 Kudos

16,446 Views
guoweisun
NXP TechSupport
NXP TechSupport

你的电路上的PC01是什么型号具体的。

假如你在输出端跟R025之间串联一个24V的稳压管,这个时候你可以要R023或者不用,但是R025建议选择在2.5K左右再试试。D302可以不用。

0 Kudos

16,447 Views
bkl
Contributor I

PCO1是VOL618A-2X001T。我直接用串阻,不加并联电阻的话,空载情况下Vref上也会有相对较多的毛刺。然后我调大稳压管,使得稳压管下方空载时电压恒值为11.42V,这样再按照240W的反馈电路去设定,由于选的431最小电流为0.4mA,并联了2K电阻。这样空载时各处毛刺很少。是否能提供下正常负载情况下Vref或光耦二极管串联电阻上的电压的波形图?

0 Kudos

16,447 Views
guoweisun
NXP TechSupport
NXP TechSupport

我没用Vref的电压波形,但是这个Vref基本不变在load 改变的时候。这些都是小信号的变动你用示波器很难捉到。

0 Kudos

16,447 Views
bkl
Contributor I

你好!

我把反馈电路上的各电阻电容都修改过,都无法消除带载Vref上的噪声,该噪声和Vka以及光耦串阻上电压波形一致。光耦并联电阻上电压变化不大,1V左右,纹波为80mV。请问是否可能是BM,LP等模式不对,或者其他地方配置有偏差?我测试了OPP,OCP和OVP,倒没有超过限制。只是不是稳定状态,例如SNSOUT,空载时burst的脉冲群个数从2-15个不固定,一直在变。

0 Kudos

16,447 Views
guoweisun
NXP TechSupport
NXP TechSupport

我看到你的原理图有一些出入在AN11801 P73 --Fig 49. Mode presetting with the values of SNSSET R2 and RSNSOUT.

Mode presetting的一些参数设定

0 Kudos

16,447 Views
guoweisun
NXP TechSupport
NXP TechSupport

另外这个噪声也可能跟您的PCB layout有关系,如果反馈回路太长也会很容易夹杂噪声进去。

0 Kudos

16,446 Views
bkl
Contributor I

我刚才详细测量了输出和Vref的关系,输出纹波为正负800mV左右,周期为88ms左右,但是纹波上面叠加了高频噪声,频率为6.48us数量级,这个高频噪声应该是Vref噪声的根源。可能是同步整流的开关噪声,我稍后再去查查。如果有好的指导意见,请指教。谢谢!

0 Kudos

16,447 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

请把原理图放到这个帖子下面吧,还有您测试的Vref of TL431的波形也贴上来。

0 Kudos

16,447 Views
guoweisun
NXP TechSupport
NXP TechSupport

你点回复我然后点击右上角的---Use advanced editor就可以添加附件

0 Kudos

16,447 Views
bkl
Contributor I

附件为波形图,加负载比空载的输出电压要低2V,同样TL431的波形中心线也对应降低一些。请确认。

0 Kudos