AnsweredAssumed Answered

imx6solosabresd do_image_wic failed

Question asked by JIANFENG SONG on May 22, 2020
Latest reply on Jun 10, 2020 by Joan Xie

您好,我在ubuntu18.04环境中,LF_L5.4.3_1.0.0生成针对imx6solo的 image,uboot等,但是最后阶段报错误,无法生成u-boot.imx,最后也无法生成需要的image等文件,不知道是什么原因,谢谢。

 

DISTRO=fsl-imx-fb MACHINE=imx6solosabresd source imx-setup-release.sh -b buildminimal
echo "UBOOT_CONFIG = \"emmc\"" >> conf/local.conf
bitbake core-image-minimal

 

jfsong@ubuntu:~/imx-yocto-bsp/buildminimal$ bitbake core-image-minimal
NOTE: Your conf/bblayers.conf has been automatically updated.
Loading cache: 100% |############################################| Time: 0:00:02
Loaded 4067 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.44.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6solosabresd"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "5.4-zeus"
TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:0275e68b0576cdefc19718e4b1977044f9f43f48"
meta-oe
meta-multimedia
meta-python = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"
meta-freescale = "HEAD:0be39721cea6e04c589a419f4bb07fabd0da6704"
meta-freescale-3rdparty = "HEAD:aea3771baa77e74762358ceb673d407e36637e5f"
meta-freescale-distro = "HEAD:ca27d12e4964d1336e662bcc60184bbff526c857"
meta-bsp
meta-sdk
meta-ml = "HEAD:435f5e984856a943986491fddd061734a0b9eba5"
meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"
meta-rust = "HEAD:5cda04c7c2158fc982502ca1e7893f71e4ca1729"
meta-gnome
meta-networking
meta-filesystems = "HEAD:aad5b3d070cd8c58828b0975cf861d8ebc90f460"
meta-qt5 = "HEAD:432ad2aa6c3a13253fefc909faba368851d21fb1"

WARNING: /home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb:do_compile is tainted from a forced run
WARNING: /home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb:do_deploy is tainted from a forced run
Initialising tasks: 100% |#######################################| Time: 0:00:02
Sstate summary: Wanted 45 Found 0 Missed 45 Current 736 (0% match, 94% complete)
NOTE: Executing Tasks
NOTE: Setscene tasks completed
ERROR: core-image-minimal-1.0-r0 do_image_wic: Execution of '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/work/imx6solosabresd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/run.do_image_wic.93572' failed with exit code 1:
INFO: Creating image(s)...

Traceback (most recent call last):
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 127, in _open_image_file
self._f_image = open(self._image_path, 'rb')
FileNotFoundError: [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'

During handling of the above exception, another exception occurred:

Traceback (most recent call last):
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 525, in <module>
sys.exit(main(sys.argv[1:]))
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 520, in main
return hlp.invoke_subcommand(args, parser, hlp.wic_help_usage, subcommands)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/help.py", line 83, in invoke_subcommand
subcmd[0](args, usage)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 220, in wic_create_subcommand
native_sysroot, options)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/engine.py", line 189, in wic_create
plugin.do_create()
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 86, in do_create
self.create()
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 179, in create
self._image.prepare(self)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 354, in prepare
imager.kernel_dir, imager.native_sysroot)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/partition.py", line 174, in prepare
kernel_dir, rootfs_dir, native_sysroot)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/source/rawcopy.py", line 68, in do_prepare_partition
sparse_copy(src, dst)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 550, in sparse_copy
fmap = api(src_fname)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 532, in filemap
return FilemapFiemap(image, log)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 350, in __init__
_FilemapBase.__init__(self, image, log)
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 86, in __init__
self._open_image_file()
File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 130, in _open_image_file
% (self._image_path, err))
wic.filemap.Error: cannot open image file '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx': [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'
WARNING: exit code 1 from a shell command.

ERROR: Logfile of failure stored in: /home/jfsong/imx-yocto-bsp/buildminimal/tmp/work/imx6solosabresd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_image_wic.93572
Log data follows:
| DEBUG: Executing python function set_image_size
| DEBUG: 49602.800000 = 38156 * 1.300000
| DEBUG: 53698.800000 = max(49602.800000, 8192)[49602.800000] + 4096
| DEBUG: 53699.000000 = int(53698.800000)
| DEBUG: 53699 = aligned(53699)
| DEBUG: returning 53699
| DEBUG: Python function set_image_size finished
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-kernel/linux/linux-imx_5.4.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/python/python-native_2.7.16.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot-tools_2019.07.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dnf/dnf_4.2.2.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/glibc_2.30.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/bison/bison_3.4.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/ldconfig-native_2.12.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/automake/automake_1.16.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/libtool/libtool-native_2.4.6.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-support/bmap-tools/bmap-tools_3.5.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/mklibs/mklibs-native_0.1.44.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/opkg-utils/opkg-utils_0.4.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-support/lzop/lzop_1.04.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/update-rc.d/update-rc.d_0.8.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/autoconf/autoconf_2.69.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/pigz/pigz_2.4.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2019.04.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/flex/flex_2.6.0.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/meta-freescale/recipes-security/optee-imx/optee-os_3.2.0.imx.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/libtool/libtool-cross_2.4.6.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/binutils/binutils-cross_2.32.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-cross_9.2.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/quilt/quilt-native_0.66.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-connectivity/openssl/openssl_1.1.1d.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kmod/depmodwrapper-cross_1.0.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/prelink/prelink_git.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/glibc/cross-localedef-native_2.30.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/bc/bc_1.07.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/parted/parted_3.2.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_git.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-devtools/python/python-pycrypto_2.6.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/opkg/opkg_0.4.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/mtools/mtools_4.0.23.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/fdisk/gptfdisk_1.0.4.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/swig/swig_3.0.12.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/dtc/dtc_1.5.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-extended/pbzip2/pbzip2_1.1.13.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/createrepo-c/createrepo-c_0.15.0.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/rpm/rpm_4.14.2.1.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/dosfstools/dosfstools_4.1.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kern-tools/kern-tools-native_git.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-kernel/kmod/kmod-native_git.bb:do_populate_sysroot', 'virtual:native:/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.45.3.bb:do_populate_sysroot', '/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-devtools/gcc/gcc-runtime_9.2.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['linux-imx', 'python-native', 'u-boot-tools-native', 'dnf-native', 'glibc', 'bison-native', 'ldconfig-native', 'automake-native', 'qemuwrapper-cross', 'libtool-native', 'bmap-tools-native', 'mklibs-native', 'opkg-utils-native', 'lzop-native', 'update-rc.d-native', 'autoconf-native', 'pigz-native', 'u-boot-imx', 'flex-native', 'optee-os', 'libtool-cross', 'binutils-cross-arm', 'makedevs-native', 'gcc-cross-arm', 'quilt-native', 'openssl-native', 'depmodwrapper-cross', 'prelink-native', 'cross-localedef-native', 'bc-native', 'parted-native', 'gnu-config-native', 'python-pycrypto-native', 'opkg-native', 'mtools-native', 'gptfdisk-native', 'swig-native', 'dtc-native', 'pbzip2-native', 'createrepo-c-native', 'pseudo-native', 'rpm-native', 'dosfstools-native', 'kern-tools-native', 'kmod-native', 'e2fsprogs-native', 'gcc-runtime', 'bzip2-native', 'expat-native', 'zlib-native', 'sqlite3-native', 'pkgconfig-native', 'gdbm-native', 'xz-native', 'readline-native', 'db-native', 'systemd-systemctl-native', 'gettext-minimal-native', 'python3-iniparse-native', 'ninja-native', 'librepo-native', 'libdnf-native', 'libcomps-native', 'cmake-native', 'python3-native', 'elfutils-native', 'binutils-native', 'linux-libc-headers', 'texinfo-dummy-native', 'm4-native', 'qemu-native', 'util-linux-native', 'ncurses-native', 'shadow-native', 'python3-setuptools-native', 'python3-six-native', 'lzo-native', 'debianutils-native', 'libsolv-native', 'libarchive-native', 'gmp-native', 'libpcre-native', 'popt-native', 'glib-2.0-native', 'curl-native', 'file-native', 'libmodulemd-native', 'libxml2-native', 'perl-native', 'dbus-native', 'nss-native', 'gtk-doc-native', 'mpfr-native', 'libmpc-native', 'attr-native', 'libgcc', 're2c-native', 'gpgme-native', 'gobject-introspection-native', 'libcheck-native', 'json-c-native', 'libtirpc-native', 'libffi-native', 'libnsl2-native', 'libcap-ng-native', 'unzip-native', 'gettext-native', 'meson-native', 'libyaml-native', 'nspr-native', 'libassuan-native', 'libgpg-error-native']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing shell function do_image_wic
| INFO: Creating image(s)...
|
| Traceback (most recent call last):
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 127, in _open_image_file
| self._f_image = open(self._image_path, 'rb')
| FileNotFoundError: [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'
|
| During handling of the above exception, another exception occurred:
|
| Traceback (most recent call last):
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 525, in <module>
| sys.exit(main(sys.argv[1:]))
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 520, in main
| return hlp.invoke_subcommand(args, parser, hlp.wic_help_usage, subcommands)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/help.py", line 83, in invoke_subcommand
| subcmd[0](args, usage)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 220, in wic_create_subcommand
| native_sysroot, options)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/engine.py", line 189, in wic_create
| plugin.do_create()
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 86, in do_create
| self.create()
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 179, in create
| self._image.prepare(self)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 354, in prepare
| imager.kernel_dir, imager.native_sysroot)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/partition.py", line 174, in prepare
| kernel_dir, rootfs_dir, native_sysroot)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/source/rawcopy.py", line 68, in do_prepare_partition
| sparse_copy(src, dst)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 550, in sparse_copy
| fmap = api(src_fname)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 532, in filemap
| return FilemapFiemap(image, log)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 350, in __init__
| _FilemapBase.__init__(self, image, log)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 86, in __init__
| self._open_image_file()
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 130, in _open_image_file
| % (self._image_path, err))
| wic.filemap.Error: cannot open image file '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx': [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/work/imx6solosabresd-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/run.do_image_wic.93572' failed with exit code 1:
| INFO: Creating image(s)...
|
| Traceback (most recent call last):
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 127, in _open_image_file
| self._f_image = open(self._image_path, 'rb')
| FileNotFoundError: [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'
|
| During handling of the above exception, another exception occurred:
|
| Traceback (most recent call last):
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 525, in <module>
| sys.exit(main(sys.argv[1:]))
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 520, in main
| return hlp.invoke_subcommand(args, parser, hlp.wic_help_usage, subcommands)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/help.py", line 83, in invoke_subcommand
| subcmd[0](args, usage)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/wic", line 220, in wic_create_subcommand
| native_sysroot, options)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/engine.py", line 189, in wic_create
| plugin.do_create()
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 86, in do_create
| self.create()
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 179, in create
| self._image.prepare(self)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/imager/direct.py", line 354, in prepare
| imager.kernel_dir, imager.native_sysroot)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/partition.py", line 174, in prepare
| kernel_dir, rootfs_dir, native_sysroot)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/plugins/source/rawcopy.py", line 68, in do_prepare_partition
| sparse_copy(src, dst)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 550, in sparse_copy
| fmap = api(src_fname)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 532, in filemap
| return FilemapFiemap(image, log)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 350, in __init__
| _FilemapBase.__init__(self, image, log)
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 86, in __init__
| self._open_image_file()
| File "/home/jfsong/imx-yocto-bsp/sources/poky/scripts/lib/wic/filemap.py", line 130, in _open_image_file
| % (self._image_path, err))
| wic.filemap.Error: cannot open image file '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx': [Errno 2] No such file or directory: '/home/jfsong/imx-yocto-bsp/buildminimal/tmp/deploy/images/imx6solosabresd/u-boot.imx'
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_image_wic) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2265 tasks of which 2252 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/jfsong/imx-yocto-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb:do_image_wic
Summary: There were 2 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

Outcomes