How many MAX_FACES_STORAGE at SLN-VIZN-IOT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many MAX_FACES_STORAGE at SLN-VIZN-IOT?

700 Views
odelmote
Contributor II

How many MAX_FACES_STORAGE at SLN-VIZN-IOT?

Can add more in SLN-VIZN-IOT?

How can affect at recognition time?

Thanks in Advance

Oscar

Labels (1)
0 Kudos
3 Replies

582 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Oscar, 

How many MAX_FACES_STORAGE at SLN-VIZN-IOT?

The number of faces that can be stored on the SLN-VIZN-IOT is 200 faces. 

How can affect at recognition time?

In general, on the SLN-VIZN-IOT the time to recognize a face is more dependent upon the model in use rather than the number of faces stored in the face database. There is a slight dip in recognition performance the more users you add, but in our testing this dip in performance has been negligible enough that we aren't concerned with it. 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

0 Kudos

582 Views
odelmote
Contributor II

Thanks Victor

    If I need 1000 or 2,000 faces.

    What do you recomend me?

    If I put a network with a 5 or 20 devices, how can I sincronize?

    Do you have SQL database access? or I can doit?

Thanks in Advance

Oscar

El 26/05/2020 a las 05:02 p. m., victorjimenez escribió:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: How many MAX_FACES_STORAGE at SLN-VIZN-IOT?

reply from Victor Jimenez

<https://community.nxp.com/people/victorjimenez?et=watches.email.thread>

in /i.MX RT/ - View the full discussion

<https://community.nxp.com/message/1317625?commentID=1317625&et=watches.email.thread#comment-1317625>

>

0 Kudos

582 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Oscar, 

Sorry for the late response, I was checking this with the design team of the solution. 

If I need 1000 or 2,000 faces.

What do you recomend me?

Unfortunately for the moment, there aren't any official recommendations on how to deal with this type of request. I apologize for the inconvenience that this might cause you. 

If I put a network with a 5 or 20 devices, how can I sincronize?

Do you have SQL database access? or I can doit?

We don't have any official support for this either. You will have to implement this on your own. 

Regards, 

Victor 

0 Kudos