Hi,I want to know whether LS1046A and LS1088A support eLBC(enhanced local bus controller) or not.
If they don't support eLBC,could I use other ways or Bus to achive the same function just like eLBC does?
Looking forward to your answer,Thanks! ^-^
eLBC is not supported, IFC(integrated flash controller) is integrated.
IFC is used to interface with external asynchronous NAND flash, asynchronous NOR
flash, SRAM, generic ASIC memories, and EPROM. The IFC has the following general
features:
• Flash controller with seven chip-selects
• Supports error and debug registers
• Functional multiplexing of pins between NAND, NOR, and GPCM
• Supports memory banks of sizes up to 256 MB (for NOR and GPCM)
• Write-protection capability for NAND and NOR devices
• External transceiver enable/disable control on per-bank basis
Thanks for your answer!
And is there any way that we could connect a FPGA with LS1046A/LS1088A without eLBC?
Waiting for your answer.^_^
Thanks for your answer! It's a very nice answer for my question.