S32V234 2x Video interface unit (VIU) for camera input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32V234 2x Video interface unit (VIU) for camera input

832 Views
adnan
Contributor I

Hello,

I would like to know about the 2x Video interface unit (VIU) for camera input available on the S32V234 SoC. What kind of input format does these two interfaces support? Does these interfaces support camera input in the following format? 8-Bit Parallel in BT.656 format? Please check the attached picture

Thank you

Tags (1)
0 Kudos
1 Reply

779 Views
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem  is
done only via tickets. This Community is not appropriate for questions
of this kind. If you wish to receive feedback from NXP Technical Support
with respect to this question, please open a Support Case.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos