Hi, everyone. The operation is fairly simple: install the aforementioned LSDK as per the instructions, add support for multilib as in meta-imx/README file, and then bitbake fsl-image-networking-full. No additional changes made. This is an image for LS1046ARDB.
require conf/multilib.conf
MULTILIBS = "multilib:lib32"
DEFAULTTUNE_virtclass-multilib-lib32 = "armv7athf-neon"
IMAGE_INSTALL_append = " lib32-glibc lib32-libgcc lib32-libstdc++"
Running transaction test
Error: Transaction check error:
file /lib/cpp conflicts between attempted installs of lib32-cpp-9.2.0-r0.armv7at2hf_neon and cpp-9.2.0-r0.aarch64
file /usr/lib/libc.so conflicts between attempted installs of lib32-libc6-dev-2.30-r0.armv7at2hf_neon and libc6-dev-2.30-r0.aarch64
file /usr/lib/libc_nonshared.a conflicts between attempted installs of lib32-libc6-dev-2.30-r0.armv7at2hf_neon and libc6-dev-2.30-r0.aarch64
file /lib/libgcc_s.so conflicts between attempted installs of lib32-libgcc-s-dev-9.2.0-r0.armv7at2hf_neon and libgcc-s-dev-9.2.0-r0.aarch64
Tried with IPK instead of RPM (just more used to it) - similar issue. No much helpful information on the internet. Help will be greatly appreciated.
My actual problem was that I was working on the currently latest repo commit of Zeus LSDK. When I switched to an older repo commit (just work with the instructions in readme, but before repo sync replace the default.xml file in .repo directory with the older one) it behaved way better, and I'm able to build a 32bit supporting target with the following lines in my local.conf file and some minor additional fixes:
require conf/multilib.conf MULTILIBS ?= "multilib:lib32" DEFAULTTUNE_virtclass-multilib-lib32 ?= "armv7a" IMAGE_INSTALL_append = " lib32-glibc lib32-libgcc lib32-libstdc++"
yipingwang and anyone from NXP support, FYA and thanks for your work, I really appreciate that.
Please refer to the following configuration.
require conf/multilib.conf
MULTILIBS = "multilib:lib32"
DEFAULTTUNE_virtclass-multilib-lib32 = "armv7a"
Please refer to https://community.nxp.com/thread/445380 .