NXP Pico iMX7D - help with the product

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Pico iMX7D - help with the product

1,053 Views
hkasistan2408
Contributor I
How many amps is required to work with a 5v power bank (camera and wifi will use everything)


I want it to run automatically when the apk device I make is powered.
I don't want to start from the Android Thing console app
I want help with how to set up the device with Android studio.
Labels (1)
0 Kudos
1 Reply

985 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hüseyin

for i.MX7D power consumption one can look at

i.MX 7DS Power Consumption Measurement

Please note that this board is third party board not supported by nxp,

for additional details one can post question on

https://www.technexion.com/support/ 

For android one can look at

https://shop.technexion.com/pico-pi-imx7-startkit-rainbow-hat.html?SID=hvei0vcb2efa18uq5em3m0ebt6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos