AnsweredAssumed Answered

Unable to receive Read Attribute response for IAS Zone Status in JN5189 coordinator

Question asked by Bharadwaj Kollepara on May 8, 2020
Latest reply on May 19, 2020 by Mario Ignacio Castaneda Lopez

I am working with jn5189 as wireless connectivity zigbee coordinator (iot-control-bridge )and I am trying to read IAS zone status for an IAS device, but when ever I send a Read attribute request from the zgui tool I am receiving the following raw data " 1 81 0 0 c 7e 6 b1 5b 1 5 0 0 2 0 19 0 0 0 0 " in this RAW packet I don't see the zone status, but when I am checking the ZigBee sniffer I am seeing the the end node is receiving the read attribute request and giving a read attribute response with the current zone status. But I don't see that in the received RAW packet, can anyone tell why is this happening ?

Outcomes