AnsweredAssumed Answered

Which pins are available for Analog inputs in i.MX RT1050?

Question asked by Ramanathan SG on May 8, 2020
Latest reply on May 8, 2020 by jeremyzhou

Hi,

 

I am using the MIMXRT1050 EVK board where i am limited to use Analog inputs at J23 connectors. 

 

Could anyone answer the following questions:

1. What are pins I can use for analog input? I hope all GPIO pins are not compatible with analog inputs!!!! 

2. Which pins are mapped with which ADC channels out of ADC0 & ADC1?

3. How do I configure pins as analog input other than what is there in example code?

 

In manual, it says 20 channels are available for ADC. What are all pins that can be used for Analog inputs? I need more than10 analog inputs to configure at a time and use. Please provide the pins which are compatible to use as analog inputs and their corresponding ADC's. How to configure in pin_mux.c? If any manual to refer to utilizing analog inputs on i.Mx RT1050 would be helpful.

 

Example code is working fine "adc_etc_hardware_trigger_conv.c" for two analog inputs.

Outcomes