Refer to the following two links
Does QN9080 / QN9090 support any location( AOA/AOD...)?
Does QN9090 also have any plans to support localization at this time?
Hello,
Currently the only one with support would be the KW36/35.
Sorry for the inconveniences this might cause you.
Regards,
Esrtephania
Hello,
As mentioned in the post you are referencing, there are no plans to support AoA or other localization on the QN9080 at this time.
However there is limited support of localization on the KW36 family using time of flight. There is no demo software available in the SDK, but there are APIs are available to access the hardware.
See this Community Post: https://community.nxp.com/thread/501844 and this training material for the KW36: https://community.nxp.com/docs/DOC-341844
Regards,
Estephania