Hi, everybody:
There is a problem in using NT3H2111.
I use the pass-through mode, and the SRAM_PROT bit is set.
I can write and read the SRAM of NT3H2111 using CLEV6630A in pass-through mode.
I can't read the SRAM when using a phone, but I can write it.When the SRAM_PROT bit is clear, I can read it.
Look forward to your reply. thanks!
Hi Bruce Lee,
We provide an app note on that topic, please kindly refer to https://www.nxp.com/docs/en/application-note/AN11579.pdf for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------