AnsweredAssumed Answered

Reading code (my own) using the True-Time Simulator

Question asked by John Pizzuto on Apr 7, 2020
Latest reply on Apr 9, 2020 by ZhangJennie

HI, I'm using Metrowerks CW v3.1 with v6.1 True-Time Simulator, working with a 9s12c32.

I revived an old project and forget what version of my code I have working on the target pcb.

Is there a way to read the code, so I can compare it to my project files?

I don't know if it makes a difference, but I use assembly.

I connected my PE Multilink USB programmer and powered up the board, then established a connection and clicked F5, and it's running.

The True-Time Simulator is showing the last project in the "Source" window, which is unrelated to the code I want to read from the target.

I don't want to accidentally erase the device.

 

Thanks for any help.

 

JohnP

Outcomes