Hello,
The datasheet for the MPXV5010 pressure sensor only states the accuracy over a temperature range of 0-85oC. Can you provide any data about the accuracy of the MPXV5010 pressure sensor over a narrower temperature range? Preferably 15-40oC?
Thank you for your help.
Hi,
MPXV5010 is temperature compensated on the range from 0 to 85oC, the amount of error (accuracy) caused on this complete range is the same. Check the “Temperature Error Band” image on page 6 of the datasheet (https://www.nxp.com/docs/en/data-sheet/MPX5010.pdf), here you can find that the error multiplier on the complete operational temperature range, and for the range from 0 to 85 is the same as 15-40oC (multiplier of 1).
Regards,
Jose
NXP Semiconductors