CAAM support in LS1027/1028??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAAM support in LS1027/1028??

687 Views
milan_joshi
Contributor I

Is CAAM is supported in LS1027/1028?

0 Kudos
2 Replies

600 Views
milan_joshi
Contributor I

Hi ufedor,

Thanks for responding to this, it is helpful.  I understood that there is SEC5 in LS series which is somewhat different than the HAB/AHAB in case of i.MX family.

0 Kudos

600 Views
ufedor
NXP Employee
NXP Employee

CAAM = Cryptographic Acceleration and Assurance Module

Also know as SEC (security engine).

There is no public revision of the LS1028ASECRM yet.

The LS1028A SEC is based on the LS1043A SEC, so it is possible to use the LS1043ASECRM for initial familiarization.

https://www.nxp.com/webapp/Download?colCode=LS1043ASECRM 

Updates to CAAM for LS1028A above what’s found on LS1043A:
• Second DESA engine
• Second PKHA engine
• New features in ERA10 for AESA
• New features in ERA10 for PKHA

0 Kudos