i.MX8M GPU seems still OOM after apply patch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M GPU seems still OOM after apply patch

Jump to solution
2,405 Views
m_c
Senior Contributor I

We got patch from support case: #00266485, but seems still OOM after apply patch.

Previous report at https://community.nxp.com/thread/528002 

We lower the memory to 560M for Linux for decrease the time of duplicate issue.

vi ~/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland/weston_5.0.0.imx.bb

Add below

SRC_URI_append = "\

file://0004-Compositor-weston-memory-leak-when-set-size-value-in.patch \

"

cp ~/0001-Compositor-weston-memory-leak-when-set-size-value-in.patch \

~/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-graphics/wayland/weston/0004-Compositor-weston-memory-leak-when-set-size-value-in.patch

cd ~/yocto/build

bitbake -c clean weston

bitbake fsl-image-validation-imx

0 Kudos
1 Solution
2,193 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

 

solution was sent via mail.

 

Best regards
igor

View solution in original post

0 Kudos
6 Replies
940 Views
jbui
Contributor I

Hi Igor

Is it possible to have the fix attached to this post or can also send to my email?

I want to see if it fix an issue we see on our devices as well.

Thank you.

0 Kudos
1,870 Views
DC95
Contributor I

I also encountered the same problem. How did you finally solve it?

0 Kudos
2,194 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

 

solution was sent via mail.

 

Best regards
igor

0 Kudos
2,193 Views
story
Contributor II

I also encountered the same problem with gpu in imx8mm, can you give me the relevant path?

hufan105@163.com

0 Kudos
2,193 Views
m_c
Senior Contributor I

I saw it and test it on my own, seems issue has been fixed. Once customer confirm, will close this issue. Thank you for your support.

0 Kudos
2,193 Views
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

I will recheck and update.

Best regards
igor

0 Kudos