LVDS to RGB converter for iMX 6 and iMX 8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS to RGB converter for iMX 6 and iMX 8

1,596 Views
vaisago
Contributor I

I am designing a board which can harvest the functions of the Apalis iMX Som modules. The Som which I am planning to use are having iMX 6 and iMX 8 modules. I need to incorporate a 24 bit RGB display but I have only unused LVDS interface in the design. I am looking for a LVDS to RGB converter, this converter should be compatible with the iMX6 and iMX 8 (the converter must work in the frequency of the LVDS output from the iMX module). It would be so helpful if  anybody can help me in this situation to find an appropriate LVDS to RGB converter, as a solution for this issue?

0 Kudos
1 Reply

1,521 Views
igorpadykov
NXP Employee
NXP Employee

Hi VAISAG

I am afraid such devices are not supported in nxp bsps, in general one can use

any lvds de-serializer like DS90CF3x6 or other.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos