AnsweredAssumed Answered

android8.0 imx6q startup time

Question asked by 贻才 林 on Apr 2, 2020
Latest reply on Apr 3, 2020 by igorpadykov

Now we use imx6q to develop our product on android 8.0 ,and the display is output  720p by lvds.

Then, the application startup time is not fast wheather cold boot or hot boot.

We use blank application to test startup time , the average of cold boot value is  1342ms, the average of hot boot value is  485ms. 

How to optimize the application time to reduce time cost?I think it maybe optimize GPU code to solve it.

Thanks.

Outcomes