AnsweredAssumed Answered

Can we have both USB and BLE functionality on QN908x Chip simultaneously

Question asked by Ankur Rathi on Apr 2, 2020
Latest reply on Apr 6, 2020 by Ankur Rathi

I want to try both USB and BLE functionality on QN908x development board.
Individually, I am able to run HID mouse example code for USB as well as BLE from SDK2.2.1.
But, I want to have both the functionality in the same firmware.
May be different switch press will result in QN908x kit as either USB device or BLE device, depending on the which Switch press.
I was not able to find an example source code which has both the functionality in same firmware.
Is there any source code which has both the feature or is there any document which I can refer to build this.

Outcomes