AnsweredAssumed Answered

How can I import [.dbc] files into an S32DS?

Question asked by Minsik Choi on Apr 2, 2020
Latest reply on Apr 3, 2020 by Lukas Zadrapa

Dear supporters

 

I control S32K144 using S32DS. I'm currently implementing a CAN communication system, and I have a question.
I have a [DBC] file, and I need to configure the source according to the message information in that [DBC] file. It doesn't matter if I only create a CAN system once, but if I do need to create multiple CAN systems, inputting the information from the [DBC] file is quite inefficient.
So I'm curious, is there any way you can call up [DBC] files from S32DS and extract the information inside them?
Ultimately, I want to create a function that allows me to set up buffers and store medium components on my own if I just import any [DBS] file.

 

Thank you.

Minsik.

Outcomes