IMX8 HDMI 120Hz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 HDMI 120Hz?

630 Views
james_kim
Contributor II

Hi,

Does IMX8 MDMI 1920x1080P 120Hz support it?

James 

0 Kudos
1 Reply

550 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello James,

The BSP does not support this resolution software wise.

However, it would require a Pixel Frequency of 297 Mhz, which is well within the limits of the controller and within the CEA861-F Timing Summary (table 15-6 of the Reference Manual) valid frequencies, and this resolution is should be supported by the HDMI 2.0a standard, so the hardware should be able to achieve, you would need to work on the software implementation.

I hope this helps!

Regards,

0 Kudos