關於MFRC630

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

關於MFRC630

622 Views
jay_lai
Contributor I

請教各位MFRC630 Reader的Code size大小

能否用在LPC804 MCU上?

0 Kudos
1 Reply

558 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. The Basic Discovery Loop example of the Reader Library provided by NXP  (CLRC663), after the compilation process, shows a used size of the flash of approximately 113,404 Bytes. The MFRC630 is a derivative product of the CLRC663, so it is almost the same size.

 

Still, consider that the LPC804 has up to 32 KB on-chip EEPROM based flash programming memory, so the size might not be enough for your application,

 

Best Regards,

Ricardo

0 Kudos