Regarding using independent PWM mode in S12ZVML64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding using independent PWM mode in S12ZVML64

532 Views
pratibhasurabhi
Contributor V

For some testing purposes

I would like to turn on all high sides and all low sides drivers [ie gate signals] in independent mode

eg All high side on and a single pulse[PWM with xx% duty ] on all low sides -one shot scenario or low side on and PWM pulse on high side.

Query is is this possible in independent mode? or is it possible on the other[complementary mode].

If so , what all settings need to be performed.

Or is there a feature in the MagniV S12 ZVML MCU which prevents both switches from turning on at the same time? 

Thanking in advance

Labels (1)
Tags (3)
0 Kudos
1 Reply

467 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Pratibha,

There is a feature that prevents that.
GDUv4 does not have this SR mode that allows that.

pastedImage_1.png

pastedImage_2.png

pastedImage_4.png

But you can test it on GPIOs.
If this is any help.

pastedImage_5.png

Regards,
Daniel

0 Kudos