AnsweredAssumed Answered

Demo Bare board project for S32V234 SBC

Question asked by Gurmeet Singh on Mar 28, 2020

Hi Community,

 

I am evaluating the S32V234 in one of the safety-critical applications where I cannot go with the Linux/FreeRtos. So I am trying to bring up the bare board application first where I am having a hard time using the DDR configuration tool for the S32V234(lots of the compilation errors the tool generated .C and .H files). I have gone through multiple app notes and TRM(HOWTO: Use DDR Configuration and Validation Tool (S32DS for Vision)) but no luck. I am using the S32V234 SBC board with PE micro multilink debugger. The following are my requirements.

 

1. All the five cores, M4, A53_1, A53_2, A53_3, A53_4, and DDR working at maximum possible frequencies.

2. M4 core is the primary core and boots from the TCM/RAM which configures the system clocks, DDR and other system resources.

3. A53_x cores boot from the DDR(0x8000_0000 to 0x9000_0000 for code memory) with the virtual and physical address 1:1 aligned, I mean *(uint32_t*)0x80000000 on A53 cores should access to the first location of the DDR.

 

Is it possible for an FAE to share an example S32 studio project or guide on this?

Outcomes