AnsweredAssumed Answered

Unable to write to COP

Question asked by Evan Griffith on Mar 26, 2020
Latest reply on Apr 8, 2020 by Evan Griffith

Hi,

 

I am trying to implement a watchdog timer in my code, and I think the register is being addressed before I use the init function, but I can not find where.  I was able to find the disable in the system_MKL17Z644.h file:

 

#ifndef DISABLE_WDOG
  #define DISABLE_WDOG  0
#endif

 

However when I set the define to 0 I get a working watchdog timer, but not with the settings that I am sending.  I am trying to set the debug bit, and the long timeout bits as I would like as long of a timeout as I can set to start with, but when I read the register after I write to it, I only see that COPT has been set to 11, all other bits are 0.  This is read through a PE Micro debugger. 

 

For reference, here is a sample of what i cam doing to enable the COP, my actual code is way to big to just paste in. 

 

#include "fsl_cop.h"
#include "fsl_rcm.h"

 

cop_config_t configCop;

COP_GetDefaultConfig(&configCop);  //Here is where I setup the long delay and debug bits

COP_Init(SIM, &configCop);

 

No matter when I check the register, I see the same settings, that is at the top of main, right before and right after the init(). 

 

Does anyone have any ideas as to what I am doing wrong?

 

Thanks!

Outcomes