Hi,
I use LS1043ARDB board and LSDK1906 want to start the file system by mounting it over NFS,
But there is no description in the LSDK1906 manual ,
I would like to ask if there is a detailed description of the documentation.
Thanks,
Dana
Hello Dana,
After deploying rootfs on NFS server, please configure bootargs as the following
=>setenv bootargs root=/dev/nfs rw nfsroot=<tftp_serverip>:<nfs_root_path> ip=<board_ipaddr>:<tftp_serverip>:<your_gatewayip>:<your_netmask>:<board_name>:<ethx>:off console=ttyS0,115200
=>saveenv
<ethx> is the port connected on the Linux boot network.
=>tftp 0xa0000000 Image
=>tftp 0xb0000000 <dtb_file>
booti 0xa0000000 - 0xb0000000
Note:
a. On the Linux host NFS server, add the following line in the file /etc/exports:
nfs_root_path board_ipaddress(rw,no_root_squash,async)
b. Restart the NFS service:
/etc/init.d/portmap restart
/etc/init.d/nfs-kernel-server restart
Thanks,
Yiping