AnsweredAssumed Answered

How to compile C code on imx6 platform

Question asked by Edward Woeste on Mar 25, 2020
Latest reply on Mar 25, 2020 by karan gajjar

I have imx6 SABRE platform. I used this link to  create Linux image from CodeAurora that is now running on successfully on the imx6 platform. 

Task #1 - Download the source code 

 

I am building imx-image-multimedia.

 

Now I have custom test code I want use to test Wi-Fi modues.  I would like to compile this code on the imx6 platform itself.  However the Linux OS does not have and gnu compilers that I can find.  I would like to simply use g++ or arm-linux-androideabi-g++.    

 

Which compilers are present on the platform or how do you suggest I compile this code?  

 

regards

Outcomes