LPC54608 eva board ISP,SDRAM pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 eva board ISP,SDRAM pin

516 Views
実奥山
Contributor II

CPU packege is 180-pin, TFBGA  in OM13092 board

C8 pin is connected to SDRAM and ISP switch.

There is a 2.2K resistor(R108) between the ISP switch and the CPU.

Why are you using a 2.2K resistor?

Shouldn't it be a 0 ohm resistor?

Labels (1)
0 Kudos
1 Reply

411 Views
carstengroen
Senior Contributor II

My guess would be to protect the CPU if the ISP switch is pressed while the pin is used for accessing SDRAM. The 2.2K resistor will limit the current if switch is pressed during SDRAM access, at the same time its value is low enough to pull the pin low during boot (and activate ISP)