MRF101AN NEAR FM BAND PERFORMANCE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRF101AN NEAR FM BAND PERFORMANCE

839 Views
silicontechnolo
Contributor I

MRF101AN: 100 W transistor. 

Regarding reference circuit 87 to 108 Mhz.. can i use it at 76 to 87 Mhz? what is the frequency response in that band? output power? If not, can NXP support in modifying component values ( I want to use ready kit)in reference design?

Labels (1)
0 Kudos
1 Reply

769 Views
LPP
NXP Employee
NXP Employee

Reference circuit 87 to 108 Mhz would require some tuning to be used in your target frequency range.
You have created support ticket #00266185 on this topic. I will continue discussion there.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos