iMX8M mini + PCA9450

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8M mini + PCA9450

1,022 Views
giacomobiancala
Contributor I

Hi,

I am developing custom board based on iMX8M mini + PCA9450.

Is it possible to use internal RTC with backup battery? I suppose there is no possibility on PCA9450.

Is it necessary to use external RTC I2C IC?

Thanks,

Giacomo

Labels (1)
0 Kudos
2 Replies

866 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giacomo

I believe you are right, as PCA9450 has not separate LICELL input as for example

PF4210.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

866 Views
giacomobiancala
Contributor I

Thank you Igor!

0 Kudos