SPC5748G how to add Z 4_0core、Z4_1core project on the Z2 single core project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5748G how to add Z 4_0core、Z4_1core project on the Z2 single core project

Jump to solution
688 Views
longfeiwang
Contributor III

  how to add Z 4_0core、Z4_1core project on the Z2 single core project ? Single-core(Z2) engineering was used for early development,Now i want to add two more cores(Z4),Is there a specific operation method?

0 Kudos
1 Solution
575 Views
stanish
NXP Employee
NXP Employee

Hello LongFei,

in my opinion it is easier to create a new multicore project using S32DS New Project Wizard and transfer all the Z2 core source code / settings into the new project. The multicore project composes from 3 projects per core.

This way you will have fully functional multicore project with Debug configuration that allows multicore debugging.

Hope it helps.

Stan

View solution in original post

2 Replies
576 Views
stanish
NXP Employee
NXP Employee

Hello LongFei,

in my opinion it is easier to create a new multicore project using S32DS New Project Wizard and transfer all the Z2 core source code / settings into the new project. The multicore project composes from 3 projects per core.

This way you will have fully functional multicore project with Debug configuration that allows multicore debugging.

Hope it helps.

Stan

575 Views
longfeiwang
Contributor III

THKS  problem has been solved

0 Kudos