Hello everyone
My development board is IMX6Q-sabresd, and the version of my linux operating system is: 3.14.52.
Now I want to use my debug serial port as a normal serial port to transfer data. I changed console = ttymxc0 to console = error under uboot. With this modification, the debug serial port can be used as a normal serial port to communicate. But at startup, the init process will print some information to my lvds screen. This makes customers look uncomfortable.
Later I modified the configuration options of the kernel:
Configuration before modification:
CONFIG_FRAMEBUFFER_CONSOLE = y
CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY = y
CONFIG_FRAMEBUFFER_CONSOLE_ROTATION = y
Modified configuration:
# CONFIG_FRAMEBUFFER_CONSOLE is not set
After the modification, the init process does not print information to my lvds screen, but my logo is not displayed on the screen when I boot up.
Is there any good solution to my current problem?
Hello
Below nxp linux repository
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_galinux-imx - i.MX Linux kernel
dts example with uart2
imx6q-arm2.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
About the u-boot logo you can refer to the thread in our community: Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... .
Hope this can help you.