Analog video decoder driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Analog video decoder driver

Jump to solution
966 Views
s-kanda-pb
Contributor I

I'm looking for analog video decoder driver for AK8859 on Linux.

I plan to use AK8859  with i.MX6 Solo through CSI I/F and connect to analog  camera.

I found a driver for ADV7180, Although  I cannot find for AK8859.

Is there any drivers for AK8859 or sample code?  

Thanks,

Labels (3)
0 Kudos
1 Solution
836 Views
igorpadykov
NXP Employee
NXP Employee

Hi s-kanda-pb

you are right, AK8859 is not supported in nxp bsps, however adv7180

driver may be used as starting point. One can check nxp linux  documentation on
i.MX Software and Development Tools | NXP 

Also may be useful:

15. i.MX Video Capture Driver — The Linux Kernel documentation 

https://community.nxp.com/docs/DOC-332679 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
836 Views
s-kanda-pb
Contributor I

Hi. igor,

OK. I will confirm to ADI and other decoder makers.

Thanks,

0 Kudos
836 Views
s-kanda-pb
Contributor I

Hi.  igor,

Thank you for your reply and I understood.
I have two more question.


1.There some variation of ADV7180. "ADV7180BSTZ"(6ch input/8or16bit output) is specified in SABRE board's BOM.
   Is other variation (i.e. ADV7180KCP32Z,ADV7180BCPZ,ADV7180WBST48Z) supported by BSP?
   6ch input is too many for us.

2.According to ADI Web site.ADV7180 is no longer  recommended for new design. Do you know any other analog decoder which supported by BSP and Video4Linux.

Regards,
S.Kanda

0 Kudos
836 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kanda

1. supported ADV7180 part (ADV7180BSTZ) can be found in BOM file of  SABRE-AI-BASE-BOARD

Design files for Base Board

2.>Do you know any other analog decoder which supported by BSP and Video4Linux.

not sorry.

Best regards
igor

0 Kudos
837 Views
igorpadykov
NXP Employee
NXP Employee

Hi s-kanda-pb

you are right, AK8859 is not supported in nxp bsps, however adv7180

driver may be used as starting point. One can check nxp linux  documentation on
i.MX Software and Development Tools | NXP 

Also may be useful:

15. i.MX Video Capture Driver — The Linux Kernel documentation 

https://community.nxp.com/docs/DOC-332679 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos