AnsweredAssumed Answered

I can't bind new endpoint to the router base device example

Question asked by Alvaro Velazquez Salas on Mar 9, 2020
Latest reply on Mar 17, 2020 by Mario Ignacio Castaneda Lopez

Hello.

 

I'm new developping ZigBee software and I have the FRDM-KW41Z microcontroller.

I've started with de router base device example and the end sleeping base device and it works fine.

 

Then I've add a new endpoint to the router following the instruction posted in the link below:

ZigBee 3.0: Adding Endpoint on KW41Z 

 

Finally I tried to bind one of the new endpoint to an another router base device with no modifications but it doesn't work.

This is the only modification I've done apart from the changes to add the endpoint and define BDB_SUPPORT_FIND_AND_BIND_INITIATOR macro.

 

What am I doing wrong? Do I need to make any other changes to get the endpoints bounded?

 

Thank you so much.

 

PD: These are the debugging output from the console

/**********************************************************************************************************************/

Outcomes