hi,
I have an i.mx8mq evk with a dsi interface and a csi interface , I want to know is there any way to make csi work as dsi. Actually, I want to use CSI interface to send DSI's data.
Any answer will be helpful.
Hi 王 澳
unfortunately mipi-csi can be used only for data input, may be useful
to look at its documentation on:
MIPI Camera Serial Interface 2 (MIPI CSI-2)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igo
Thank you for your reply, by the way, if I configure CSI as DSI in the dts file, is that effective?
Let me put it another way,could CSI's hardware interface be configured as DSI? I want to use two mipi panels, sadly only one DSI on the i.mx8mq evk.
Best regards
澳刚