Hi,
I have a couple of questions.
1) Has HDMI input been enabled for MX8QM for Android OS ? If not, what is the ETA?
2) Also, what is the typical application for HDMI input? Is it possible to overlay graphics over the HDMI-input before sending it out to HDMI-out ? Essentially is it like a camera input ?
From datasheet, I see that Rx may not be enabled yet.
Datasheet : https://www.nxp.com/docs/en/data-sheet/IMX8QMAEC.pdf
HDMI-RX and SATA are not currently supported, the related power and signal connections are provided for future use when it is expected HDMI-RX and SATA support will be enabled.
Any documentation regarding above questions would be great.
thank you!
RD suggests to use Linux unit test to test this function. There is no plan to add this feature in Android as it's not within Android spec.
thanks Joan