IMX287 nicro SD card boot error 0x8020a014

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX287 nicro SD card boot error 0x8020a014

619 Views
qmark
Contributor I

Hi,

I have a new custom board base on IMX287. It should be boot from SD card(connected to SSP0). I use Kingston 16Gb micro SD CARD. When I boot, I got some information from DUART port. Please see the attached image file. First, it shows "0x8020a014", and then "HTLLCbLLJbde". wait a while, it shows
Version 12.200306.1633

************************
Hellow E1-
************************

I set character "b", "d", "e" in my boot.s file for checking and set the "Version 12...." and "Hellow E1-" in my main.c. They all displayed on the DUART.

I have set "ENABLE_SSP_12MA_DRIVE" to high ( HW_OCOTP_ROM7 ) and SSP0_CMD connect a 10K pullup resistor.

It seems the boot is successful, but I don't know why it shows "0x8020a014".

Thanks,

QL

Labels (1)
0 Kudos
2 Replies

548 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello qmark,

Looks like the SDCARD is not supported please check it:

https://community.nxp.com/thread/303344 

Regards

0 Kudos

549 Views
qmark
Contributor I

Hi Bio_TICFSL,

Thanks for your help. I checked VDD pin of micro SD card connector and found the timing of power ramp up a little longer (60 msec). I changed the capacitor and shorter the timing of power ramp up to 12 msec. Boot again, the error "0x8020a014" removed.

Thanks

0 Kudos