Hi,
I have a issue when compiling the model based code:
Error: File: C:\Users\leewe\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_MPC57xx\mbdtbx_mpc574x\mbdtbx_mpc574x\blocks\ctu\ctu_mpc574x_config.tlc Line: 130 Column: 34
Unable to find pins within the user_config scope
Can anyone help me with that?
The model is attached below.
Regards,
Lee
Solved! Go to Solution.
Hello leeewayyy,
Thank you very much for noticing this behaviour. I was able to replicate this and indeed is very strange.
However, I have updated the mbd_mpc574x_ec_toolbox.mdl file, that I was also attached to this response, so please backup the mbd_mpc574x_ec_toolbox.mdl file and then replace it with the one attached.
The file is located under [Toolbox Install Path]\mbdtbx_mpc574x\mbdtbx_mpc574x file.
Hope this helps,
Marius
Hello leeewayyy,
Thank you very much for noticing this behaviour. I was able to replicate this and indeed is very strange.
However, I have updated the mbd_mpc574x_ec_toolbox.mdl file, that I was also attached to this response, so please backup the mbd_mpc574x_ec_toolbox.mdl file and then replace it with the one attached.
The file is located under [Toolbox Install Path]\mbdtbx_mpc574x\mbdtbx_mpc574x file.
Hope this helps,
Marius
This only happens when i use CTU1 instead of CTU0.