Nitrogen 8M got bricked due to "mmc partconf 0 1 0 0" command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nitrogen 8M got bricked due to "mmc partconf 0 1 0 0" command

1,344 Views
ashoknoone
Contributor I

Hi,

I am using nitrogen 8M (boundary device board), when trying to configuration partition through U-Boot.  I have gave comand like "mmc partconf 0 1 0 0" accidentaly, after that  i am not able to see my U-Boot serial console.

So recover it, I have also tried System recovery option to flash u-boot through Serial Download. I am able to successfully the flash it, still U-Boot is not working.

I have followed following steps

1. As suggested in the below, I have built Boundary device uboot for imx8 in the Building for i.MX8 section
https://boundarydevices.com/u-boot-v2018-07/
 
2. Then pulled the latest imx_usb_loader from: https://github.com/boundarydevices/imx_usb_loader
 

And I kept both imx_usb_loader and u-boot in the same directory. Then tried to run imx_usb_loader as follows:
 

sudo ./imx_usb


3. Repeated the step again. That is-> sudo ./imx_usb 

Please check attachment, I have given the steps executed in the machine . And please help me to unbrick the devices.

Regards,

Ashok S

0 Kudos
2 Replies

1,236 Views
gary_bisson
Senior Contributor III

Hi,

Please use uuu to unbrick the device as explained here:

https://boundarydevices.com/recovering-i-mx-platforms-using-uuu/ 

Regards,

Gary

0 Kudos

1,236 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ashok S,

This board is manufactured and supported by Boundary Devices. While hopefully a community user may have experience with this board and provide some help, I would recommend that you contact Boundary Devices for help.

My apologies for the inconvenience.

Regards,

0 Kudos