i.mx53 GPU - does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx53 GPU - does not work

638 Views
alexberenshtein
Contributor III

Hi everyone.
Someone might explain, step by step, how to start the GPU in the Yocto Zeus (  i.mx53 ).

My parameter: MACHINE ?? = imx53gsb

                        DISTRO?= fscl-framebuffer

DISTRO_FEATURES_remove =" x11 wayland"

DISTRO_FEATURES_append = " framebuffer opengl gpu"

Best regards

Labels (2)
0 Kudos
1 Reply

502 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Alex Berenshtein,

In this older thread (which I’m realizing it was started by you) there is insight on pending developments, perhaps they could help:

https://community.nxp.com/message/1023052

The i.MX53 is not supported on the BSP releases, only on the Community BSP. That being said, I would recommend switching to an older branch which may have more work done. Zeus is stable but I’m not sure much work has been done on the i.MX53 as of today. You can subscribe to the mailing lists (link below for more information) to ask developers and users of the Community BSP about the status of the i.MX53 GPU support for the different Branches.

http://freescale.github.io/#contributing

I hope this information helps!

Regards,

0 Kudos