AnsweredAssumed Answered

I have questions about the MC33772 chip.

Question asked by jang junghoon on Mar 1, 2020

Hello, I would like to ask a question when testing the MC33772 chip.

 

1) Is it possible to activate Sleep-Wakeup / Fault Pin using GPIO 0 pin?
2) Overcurrent when passing 250mA or more with shunt resistance 75u ohm
     Is it possible to enable Sleep-Wakeup / Fault Pin in situations?
3) I want to set the overcurrent when the shunt resistance is set to 75 ohm and it passes over 250mA. How should I set up?

Outcomes