operating https://community.nxp.com/discussion/?keyword=" style="color: #3d9ce7; border: 0px; font-weight: inh...steps:
1、tar -xjvf ls1046-linux-fs.tar.bz2
2、cd ls1046-linux-fs.tar.bz2
3、source setup.env
4、flex-builder -m ls1046ardb -a arm64
Makefile:4772: recipe for target 'lib/dhparams.lo' failed
make[4]: *** [lib/dhparams.lo] Error 1
make[4]: *** 正在等待未完成的任务....
mv utilities/ovs-lib.tmp utilities/ovs-lib
mv -f lib/.deps/lib_libsflow_la-sflow_sampler.Tpo lib/.deps/lib_libsflow_la-sflow_sampler.Plo
mv -f lib/.deps/lib_libsflow_la-sflow_poller.Tpo lib/.deps/lib_libsflow_la-sflow_poller.Plo
mv -f lib/.deps/lib_libsflow_la-sflow_agent.Tpo lib/.deps/lib_libsflow_la-sflow_agent.Plo
mv -f lib/.deps/lib_libsflow_la-sflow_receiver.Tpo lib/.deps/lib_libsflow_la-sflow_receiver.Plo
make[4]: 离开目录“/home/iotgw/ls1046/ls1046-linux-fs/flexbuild/packages/apps/ovs-dpdk”
Makefile:5526: recipe for target 'install-recursive' failed
make[3]: *** [install-recursive] Error 1
make[3]: 离开目录“/home/iotgw/ls1046/ls1046-linux-fs/flexbuild/packages/apps/ovs-dpdk”
Makefile:5831: recipe for target 'install' failed
make[2]: *** [install] Error 2
make[2]: 离开目录“/home/iotgw/ls1046/ls1046-linux-fs/flexbuild/packages/apps/ovs-dpdk”
Makefile:120: recipe for target 'ovs-dpdk' failed
make[1]: *** [ovs-dpdk] Error 2
make[1]: 离开目录“/home/iotgw/ls1046/ls1046-linux-fs/flexbuild/packages/apps”
Makefile:30: recipe for target 'ovs-dpdk' failed
make: *** [ovs-dpdk] Error 2
make: 离开目录“/home/iotgw/ls1046/ls1046-linux-fs/flexbuild”
It looks like that this LSDK is not fully installed.
Use the following command sequence for LSDK installing:
sudo apt-get install git
sudo apt install -y binfmt-support qemu-system-common qemu-user-static
tar xvzf flexbuild_lsdk1909_update_311219.tgz
source setup.env
flex-builder -i mkrfs -a arm64
flex-builder -c linux -a arm64
Have a great day,
Pavel Chubakov
yes,its is SDK-18.06-V4.14 package!
thanks you reply!
Is Ubuntu 18 used for this LSDK?
Have a great day,
Pavel Chubakov
hi Pavel Chubakov,
thinks you help !
I use flexbuild_lsdk1909_update_221019.tgz compile, step to sudo apt install -y binfmt-support qemu-system-common qemu-user-static
that hint location qeumn-user-static package,what can i do?
iotgw@iotgw-virtual-machine:~/ls1046/flexbuild_lsdk1909_update_221019$ sudo apt install -y binfmt-support qemu-system-common qeumn-user-static
正在读取软件包列表... 完成
正在分析软件包的依赖关系树
正在读取状态信息... 完成
E: 无法定位软件包 qeumn-user-static
NXP offers flexbuild_lsdk1909_update_311219 for the LS1046ARDB and the LS1046A-FRWY boards.
Use the following command sequence for installing this LSDK under Ubuntu 18:
sudo apt-get install git
sudo apt install -y binfmt-support qemu-system-common qemu-user-static
tar xvzf flexbuild_lsdk1909_update_311219.tgz
source setup.env
flex-builder -i mkrfs -a arm64
flex-builder -c linux -a arm64
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------