Hi,
I'm using clrc663 for my project.I want to implement peer to peer functionality in my project.In NXP NFC reader library version5.22, EX3_NFC_FORUM is meant for PN5180.But i want p2p example for clrc663.Can anyone suggest me example for peer to peer communication in clrc663 and which protocol i need to use for p2p in clrc663.
Hi,
You can check the examples in the NFC Reader Library , you can check the different defines in the ph_NxpBuild_App.h to enable the peer to peer functionality. I would recommend you to check especially the Simplified_API_ISO examples and you can search for all the references to peer to peer there. Also, please notice that in the Library there is a commented line "if FE HAL is RC663, then exclude ISO14443 Card Mode PAL & ISO18092 Target Mode PAL (P2P), otherwise include as required." (ph_NxpBuildApp.h)
Could you please try using the provided information? Please let me know if you have any question.
Best Regards,
Ricardo
Hi,
You can also check this application note to help you in the process.
https://www.nxp.com/docs/en/user-guide/UM10721.pdf
Regards,
Ricardo