SCL I2C Frequency with MPC8569 in security full rate mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCL I2C Frequency with MPC8569 in security full rate mode

496 Views
vaque
Contributor II

Hi all;

I am ussing a MPC8659 microcontroller with a 400MHz platform clock (CCB). I am trying to obtain 100KHz in I2C2 SCL apliying FDR=0X2F (2048) in I2CFDR (400MHz/2/2048 = 97656Hz) yet the SCL line have 190KHz. I am ussing security full rate mode yet I can read in MCP8569ERM.pdf that it doesn't affect in I2C2.

Can you help me please? Does anyone know hot to do it right?

Best regards. Daniel.

Tags (2)
0 Kudos
2 Replies

440 Views
ufedor
NXP Employee
NXP Employee

The I2C IP is actually a dual I2C and it gets single IP clock, so both I2C controllers behave the same from the rate perspective.
There is an issue with the RM.

440 Views
vaque
Contributor II

Ok.

Thanks so much!.

0 Kudos