U-boot error in imx6qsabre board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-boot error in imx6qsabre board

1,315 Views
sheraz_ali
Contributor II

Hi 

I am using MCIMX6Q-SDP board and trying to boot 4.19 bsp using pre-built binaries provided in L4.19.35_1.1.0_images_MX6QPDLSOLOX

U-Boot 2019.04-4.19.35-1.1.0+g4d377539a1 (Oct 29 2019 - 14:53:36 +0000)

CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 26C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM: 1 GiB
wait_for_sr_state: failed sr=5 cr=98 state=202
i2c_init_transfer: failed for chip 0x8 retry=0
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
i2c_init_transfer: failed for chip 0x8 retry=1
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x23!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x23!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x31!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
i2c_init_transfer: failed for chip 0x8 retry=0
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x31!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x38!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x38!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
i2c_init_transfer: failed for chip 0x8 retry=0
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x3f!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
read error from device: 4ef41258 register: 0x46!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
read error from device: 4ef41258 register: 0x4d!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
read error from device: 4ef41258 register: 0x6a!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
read error from device: 4ef41258 register: 0x6f!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
read error from device: 4ef41258 register: 0x70!
wait_for_sr_state: Arbitration lost sr=13 cr=98 state=202
read error from device: 4ef41258 register: 0x71!
read error from device: 4ef41258 register: 0x0!
wait_for_sr_state: failed sr=0 cr=a8 state=2020
i2c_init_transfer: failed for chip 0x8 retry=0
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x3!
PMIC: PFUZE100! DEV_ID=0xfffffffb REV_ID=0xfffffffb
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x21!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
write error to device: 4ef41258 register: 0x21!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x24!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
write error to device: 4ef41258 register: 0x24!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x2f!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
write error to device: 4ef41258 register: 0x2f!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
read error from device: 4ef41258 register: 0x32!
wait_for_sr_state: Arbitration lost sr=32 cr=98 state=202
write error to device: 4ef41258 register: 0x32!
read error from device: 4ef41258 register: 0x0!
Not supported, id=11
initcall sequence 4ffc67bc failed at call 17805740 (err=-22)
### ERROR ### Please RESET the board ###

I am getting the following error,

Labels (6)
3 Replies

462 Views
welsonliu
Contributor I

Hi ,

i encounter the same u-boot issue when using imx6q, so do you solve the problem about this board?  

0 Kudos

1,147 Views
radhikasomaiya
Senior Contributor II

Hi sheraz.ali@iwavesystems.com ,

Can you please verify that the image is flashed properly or not in your sdcard? As we are able to boot the board using sdcard with prebuilt of L4.19.35_1.1.0_images_MX6QPDLSOLOX

 

Try to boot board using prebuilt from: 

https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_MX6QDLSOLOX&appType=license 

For steps You can download the document from this link and refer the section 4.3.2 and 4.3.4.

Regards,

Radhika Somaiya.

0 Kudos

1,147 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!

0 Kudos