iMX6 DualPlus/6QuadPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 DualPlus/6QuadPlus

760 Views
abhayv_bellale
Contributor I

Hi all 

can you please help Is the iMX6 DualPlus/6QuadPlus the right processor for measurement of below parameters?

Also I want to go for OS based application that needs to perform other tasks USB, ethernet, wifi, small display. 

 

  • Voltage : DC +/-1.5mV +/-50V
  • current and 4-20mA current loop (internal or external shunt)
  • resistance (2, 3, 4 wire; max 1MΩ)
  • ratiometric resistance e.g. strain gauges (1/4, 1/2 or full bridges; current or voltage excited)
  • thermocouples: types B, C, D, E, G, J, K, N, R, S, T (internal or external reference junction sensor)
  • RTDs (Pt, Ni, Cu)
  • thermistors (YS400xx series; generic thermistor scaling)
  • IC temperature sensors (AD590 series, LM35 series, LM135 series)
  • Frequency from 10Khz up to 0.45Mhz) (sine, 5Vpp,  50V input range, 0Vthreshold)
  • vibrating wire strain gauges (DT80G/85G GeoLogger only)
  • Carlson meters

Thanks,

abhay 

Labels (3)
Tags (1)
0 Kudos
1 Reply

647 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can see this

0 Kudos